Get Current Screen
Capture the current screen image from the DMM's front panel. Note that this operation captures the current screen image without initiating a new measurement. Click the "Start" button to trigger a new measurement prior to capturing a screen image. 
If Auto Refresh is enabled, the label on this button changes from "Get Current Screen" to "Start Auto Refresh".